Solution
Center of Gravity Testing for Robotics
The center of gravity represents the point where the entire weight of the robot can be considered to respond and act.
The center of gravity represents the point where the entire weight of the robot can be considered to respond and act. It is a critical factor that determines the stability and balance of a robot, especially during operation.
Interface suggests using their force plate option to install at the base of the robotic arm. Four 3-Axis Force Load Cells are installed between two force plates, then installed at the bottom of the robot. This creates one large 6-Axis Force Plate. The sensors force data is displayed and monitored with two BX8 Multi-Channel Bridge Amplifier and Data Acquisition Systems onto the customer’s PC.
Interface’s 6-Axis Force Plate was able to successfully measure the robot’s center of gravity.
Four 3-Axis Force Load Cells
Mounting Plates
Two BX8 Multi-Channel Bridge Amplifier and Data Acquisition System with supplied software
Robotic Arm
Customer’s PC
Notifications